New Four-Port Wall/Shelf-Mount and Rack-Mount Gas Tube Lightning Protectors Protect Cat 6 Lines NORTH ANDOVER, MA - 3/28/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has introduced two new gas tube lightning protectors designed to protect up to four Category 6 Ethernet cable lines. Designed to stop transient voltages or power spikes from damaging sensitive electronic equipment, these new wall/shelf-mount and rack-mount models offer even better protection than the diode versions that L-com has carried since 2009. L-com's earlier models of four-port Cat 6 lightning protectors used ultra-low capacitance diodes to stop spikes of up to 65 Volts. The new models use gas discharge tubes to provide low line-to-line and line-to-ground capacitance, minimizing distortion of high-speed signals. They stop spikes up to 90 Volts and have L-com's highest power rating available. The new parts are also compatible with 802.3af/at PoE devices. "We know that power surges cause massive expenses to businesses world-wide every year," said Patrick Pesa, Director of Product Management. "We're glad we're able to offer such high-power protection with nearly no impact at all in signal speed or quality. Now customers can easily protect high-speed Ethernet devices with the convenience of a wall or rack mount protector for up to four separate lines." The new protectors are built in the USA and stocked in L-com's Florida distribution center for shipment on the same day as ordered. Detailed datasheets for the wall/shelf-mount and the rack-mount products are available for free download on the L-com.com web site. Please click here to download a high-resolution version of the first image suitable for print publication. Please click here to download a high-resolution version of the second image suitable for print publication. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |