L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of audio/video, active optical cables (AOC) that were developed to extend high quality audio and video signals up to 100 meters without the use of a repeater.
L-com’s new AOC cables include HDMI 2.0 assemblies, 1.4 DisplayPort cables and video DVI cable assemblies. Each series features cable lengths ranging from 10 meters up to 100 meters off-the-shelf. These new long-reach AOC cables are lightweight and flexible, require no external power supply and are resistant to EMI and RFI.
The new HDMI AOC cables feature resolutions up to 4K@60Hz, compatibility with HDMI 2.0, EDID, HDR, HDCP (2.2) and multi-channel audio support. The DVI AOC cables support resolutions to 1080p and 4K2K as well as source connectors that are programmable to store EDID information. Lastly, the new DisplayPort AOC cables provide 8.1 Gbps per channel, support for 8K@60Hz, HBR3, HDCP 1.4/2.2 and a slim 4.8mm outer diameter cable.
“Many times, our customers require the extension of digital audio and video signals well beyond the various standards’ length limitations. Our new AOC cables were designed to address these types of applications where the need to extend A/V signals without the use of a repeater is a requirement,” said Paul Hospodar, Product Line Manager.
L-com’s new HDMI, DVI and DisplayPort 2.0 AOC Cables are in-stock and available for immediate shipment. In addition, check out our DVI to HDMI cables which bridges old technology with new. Check out our DVI cable to HDMI assembly and order now for same business day shipping.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, ShowMeCables, INC Installs, Integra Optics and NavePoint. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936