To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

New LC Fiber Optic Cables added to L-com Connectivity Products’ Fiber Optic line

Monday, April 16, 2007

North Andover, MA – April 17, 2007L-com, Inc., of North Andover, MA, has added two new fiber optic cable designs to its already extensive fiber optic cable assembly offering.

  • The new FODLC-UNI- series Uniboot LC assemblies provide an integrated boot and clip design as well as a single 3.0mm jacket. These unique assemblies are available in either 62.5/125 or 50/125 styles and range from 1 to 10 meters in length.

  • The FODLC-CL- series features clipped LC connectors and a duplex cable design and are available in 62.5/125, 50/125 and 9/125 styles.

  • Along with these two new LC fiber optic cable designs, L-com continues to offer their standard FODLC- duplex LC fiber cables (not clipped).

Clips on LC connectors allow the two normally separate LC connectors on a duplex cable to function as one connector. This ability is sometimes prized by engineers as a way of “fool-proofing” patching these cables, as the A and B fibers can not be mixed up. However, in other situations the LC connectors must stretch apart to reach separate ports. L-com’s product offering will now include solutions to both scenarios off-the-shelf.

In addition to the stock products, L-com also offers custom-built lengths of these and all of its fiber optic cable assemblies. The combination of short lead times and low minimum order quantities has allowed them to maintain their leadership position in the fiber optic cable assembly industry.

For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com

For over 25 years, L-com has designed and manufactured copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:

· Assembled and Injection Molded Data Cables
· Fiber Optic Cable Assemblies and Adaptors
· Modular and Telco Assemblies
· Low Loss Video and Monitor Cables
· Unique Bulkhead Connectors
· Machined or Cast Coaxial Connectors and Adaptors
· Sheet Metal Fabrication of Rack Panels and Enclosures
· Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
· Military and Special Packaging, Kitting, Custom Labeling and Bar-coding

L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit www.L-com.com.