To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

New USB 2.0 Right-Angle Type B and Mini-B5 Adapters Solve Tight Space Connection Problems

Tuesday, November 29, 2011

New USB 2.0 Right-Angle Type B and Mini-B5 Adapters Solve Tight Space Connection Problems

NORTH ANDOVER, MA – November 30, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has introduced new right-angle USB adapters featuring USB type B male to female connectors and USB type mini-B5 male to female connectors.  The new adapters allow cables to plug into USB type B and mini-B5  jacks and cables at right angles without causing damaging bends in the cable.

These right angle adapters follow other recent angled USB products including right-angled USB 2.0 cables, right-angle USB type A adapters, and USB A flexible adapters. Like previous adapter types, the new adapters come in two “exit” styles, allowing the right angle to bend in either direction relative to the connector they are plugged into. The type B adapters use 20 AWG power leads providing maximum power transfer, and both styles use 30 microinch gold contact plating to endure repeated plugging and unplugging of the cable.

“We are finding that strain on cables from bending to fit in tight spaces is an increasing problem,” said Steve Smith, Product Manager. “These adapters are more and more in demand as customers combat this issue.”

These adapters will be stocked in North America for same-day shipment on orders.  They will come molded in PVC and will be 100% shielded to protect from EMI/RFI. Engineering drawings and 3D CAD models will be available for free on the L-com web site.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/