To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

New USB Products from L-com Global Connectivity

Tuesday, April 21, 2009

North Andover, MA – April 21, 2009 –  L-com, a global leader in the manufacture of wired and wireless connectivity products today announced the release of several new Mini B 5 Position USB products for extending and connecting Mini B 5 position systems and peripherals. Adding to its Mini B 5 position USB offering, L-com has released the CSMUMB5X series male to female Mini B 5 position extension cables which are perfect for extending in Mini B 5 peripherals.  

     

 

In addition L-com has introduced an innovative USB Mini B 5 position coil cable (COILMB5EXT-2M) which features variable lengths of .5 meters to 2 meters. This cable can be used with GPS systems and other applications requiring Mini B 5 position connections.

 

Furthermore L-com has added a line of Mini B 5 position dust covers to protect unused ports. The CAPUSB-MB5 is sold in 10 piece packs and features a friction fit design.

 

For more information about this release, please contact:

Steve Smith, Product Manager978-682-6936 x1156, ssmith@L-com.com

About L-com 

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com