Nickel-plated brass flanged USB coupler provides stability and shielding
Nickel-plated brass flanged USB coupler provides stability and shielding
Tuesday, January 25, 2011
NORTH ANDOVER, MA – 01/26/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a new style USB A-B coupler made with nickel-plated brass. These new ECF504-AB couplers are supplied as an assembled kit that includes the UADKEY-AB keystone coupler and the ECF style mounting frame, along with two mounting screws.
"This is similar to our popular ECF504-UABS adapters," said Steve Smith, Product Manager, "except those use chrome-plated plastic while the new one uses nickel-plated brass. We wanted to offer our customers a full-metal option along with the existing chrome-plated plastic one."
Both the ECF504-UABS and the new ECF504-AB kits are stocked in North Andover, MA for same-day shipment.
For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450,newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/