NORTH ANDOVER, MA – 6/10/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today that Serial ATA (SATA) extension cables are now available. The new cables would allow SATA data to reach further, extending internal communication in “big box” situations.
"Our IT Manager was having difficulty connecting a bulky disk on a module to a SATA connector on a tightly packed PCB. Our new SATA extension cables solved his problem by extending the SATA connector away from the PCB, where there's more room,” said Steve Smith, L-com’s Product Manager in charge of SATA products. He said, “Plus, extension cables are handy to have for any interface. Sometimes existing cables just don't reach." These cables utilize male to female connectors, bright red PVC cable jackets and gold-plated contacts. L-com is offering both 12” and 20” lengths right now.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/