Six New NEMA Enclosures from L-com Provide Rain Shielded Ventilation
NORTH ANDOVER, MA – 3/8/2010 – L-com, Inc., a leading manufacturer of both wired and wireless connectivity products, announced today the availability of a new line of actively cooled and ventilated NEMA enclosures based on the company's extremely popular NBP141004-100 model.
In this new line of NEMA enclosures, L-com has modified its base model to include a number of heat-dissipating features, including multiple rain shielded vents and active cooling fans controlled by thermostats. These enclosures assure cooling in outdoor applications, protecting equipment from the elements and heat buildup. The new enclosures come in 120VAC, 240VAC Universal Plug EURO, and Power over Ethernet (PoE) versions.
Weatherproof Enclosures are very popular for outdoor installations because they provide great protection against ingress dust and water. These new enclosures are designed to help combat networking installers’ greatest enemy: heat, while at the same time providing maximum protection against rain and water ingress.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.comL-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/