USB 3.0 Bulkhead Cables Added to L-com Lineup NORTH ANDOVER, MA - 01/09/12 - L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has added USB 3.0 cable assemblies with a type A female bulkhead connector on one end. These assemblies are designed to be easily installed on panels or chassis and provide access to hard-to-reach or secured USB 3.0 ports. The new USB 3.0 cable assemblies use a multi-layered PCB in the bulkhead that maintains USB 3.0 speed and performance. The “ECF504” style bulkhead mounts to virtually any panel thickness via an electrically grounded flange. They are a USB 3.0 version of the original USB 2.0 cable assemblies that L-com has carried for years. USB 3.0 is up to ten times faster than USB 2.0, with speeds reaching 4.8 Gbps. Steve Smith, Product Manager, said, “The new USB 3.0 cable assemblies will allow design engineers to create products utilizing the drastically-improved speed of the latest USB standard with a pre-terminated bulkhead connector that is simple to install.” For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com Please click here to download a high-resolution version of the image suitable for print publication. L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |