NORTH ANDOVER, Mass. (March 17, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of Type-C USB 2.0 and USB 3.0 adapter cables.
L-com's adapter USB Type-C cables provide a quick and easy way to connect older peripheral devices to a new computer, or to connect new peripherals that use a Type-C connector to an older computer system.
Each series of USB cables feature simple “plug & play” connections to handheld devices and other peripherals where a Type-C to alternative USB type connections are required. Twisted pair data lines help reduce crosstalk and maximize cable flexibility.
The USB 2.0 adapter cables are available in the following configurations:
- Type-C to A
- Type-C to B
- Type-C to Micro-B
- Type-C to Mini-B 5 position
- Type-C to C for low-speed applications
The USB 3.0 adapter cables are available in the following configurations:
- Type-C to A
- Type-C to B
- Type-C to Micro-B
"These cables save customers time and money by providing a simple way to adapt the new USB Type-C standard/interface to older devices without the need to upgrade them. They also provide a straightforward method of converting Type-C connectors to alternative USB formats without the use of an adapter,” said Dave Gallagher, Product Manager.
Each series of these new adapter cables is offered off the shelf in six stock lengths. They feature 30u gold-plated connectors for repeated mating cycles, a double-shielded cable for EMI/RFI protection and fully molded connectors for strain relief.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/