Blog posts tagged with 'ethernet-cables'

Benefits and Applications of Single-Pair Ethernet Cable
Internet-connected devices with advanced sensor and control features are becoming increasingly common in industrial applications. The rise of the industrial internet of things (IIoT) is being driven by the availability of more capable wired and wireless connectivity technologies and the need for manufacturers to enhance efficiency, reliability, and productivity through automation.... Read more
High-flex Ethernet Cables: Applications & Overview
In the world of industrial Ethernet and building automation, there is a bountiful opportunity for very harsh environments and challenging installation situations. In these cases, industrial Ethernet rated cables are often used. These ruggedized Ethernet cables tend to have additional shielding thickness, thick and hard outer jackets, strain relief members built in, and other protections for the delicate copper wiring... Read more