It’s no mystery why fiber optic technology has grown in popularity since it was commercially introduced in the 1970s. Sending data via infrared light pulses on a fiber line, rather than electrically over copper cable, allows the transmitting of more information faster, over longer distances and with no threat of radio or electromagnetic interference. That’s why it is often the choice for ....... Read more