Blog posts tagged with 'ip67'

IP65, IP66, and IP67 Ratings for Water Protection: So, What’s the Difference?
Ingress protection, or IP, standards dictate the level of water and fine particulate protection for components and equipment enclosures. Significant differences exist between water resistant, waterproof, and other labels—but what do each of the actual IP standards mean?... Read more
M12 Connector Coding Demystified
When you need to ensure that you have a reliable connection, even in the harshest conditions, you need an M12 connector. These rugged ....... Read more