A Multi-fiber Push On (MPO) connector is a fiber optic connector that contains multiple fiber-optic lines internally. MPO connectors are used for high-speed telecommunication and data communication networks. The standards governing the design and use of MPO connectors are the IEC 61754-7 and TIA 604-5. Originally, MPO connectors were predominantly used in the Central and Branch offices but have also seen wide adoption in high performance computing (HPC) applications and in enterprise datacenters.... Read more