To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

Blog posts tagged with 'poe+'

PoE Switches vs PoE Injectors – What To Use When
Power over Ethernet (PoE) delivers power and data to PoE-enabled devices over the same ethernet cable. Ethernet cables contain 4 pairs of wire, but most networks only use 2 of the pairs for data transmission. PoE uses the 2 unused pairs of wire to provide DC power to the device. This allows the deployment of PoE compatible devices in locations that lack electricity. Since this eliminates the need to run separate power lines, PoE saves money in materials and installation time.... Read more
The 6 Essentials for Protecting Your Ethernet/PoE Network
The use of power-over-Ethernet devices has grown dramatically in recent years, especially with ratification of the IEEE 802.3bt standard in 2018. Endspans and midspans designed under this new standard can deliver up to 100 watts of power to devices, using all four wire pairs of a Cat6 Ethernet cable. Benefits of this improvement include…..... Read more