A new frontier of wireless technology is under exploration. Though we are still in the initial phases of defining everything the fifth generation (5G) wireless network will offer, we do have a glimpse into what technological wonders await. Like the generations that came before it, 5G is shaping up to be an exciting new frontier in wireless communication. Here is a look at what is in store.
Of course 5G is slated to be faster than 4G, but instead of faster peak connection speeds, the goal of 5G is a higher capacity of 20 Gbps speeds and 1 millisecond (ms) latency which would allow more users per area unit and higher consumption of unlimited data. This would make it possible for more people to stream high-definition media on mobile devices for long periods of time without a Wi-Fi connection. 5G will use OFDM encoding, which is similar to the LTE coding used by 4G but with more flexibility and lower latency. 5G may also integrate Wi-Fi as part of a cellular network, or use LTE Unlicensed which transmits LTE-encoded data over Wi-Fi frequencies.
Rather than huge towers covering long distances, 5G networks are likely to consist of small cells, some as small as home routers. This is partly because of the characteristics of the frequencies 5G will use, but mostly it is to allow for greater network expansion capacity. Using numerous smaller cells means that 5G will also have to be much more intuitive than previous generations in order to juggle all of the cells and keep up as they change size and shape. These small cells may also have more autonomy and be able to choose how and where to route data, which can significantly lower latency. Even with smaller cells, it is expected that 5G will still be able to increase capacity by four times over 4G networks by utilizing advanced antenna technologies and wider bandwidths.
The first steps for 5G will mostly like be home internet applications but with a much wider availability than closely related millimeter-wave fixed wireless IPs. For some providers, 5G may replace DSL to allow the company to offer a package deal that includes 5G home internet, satellite TV, wireless phone and home phone together.
Driverless cars may be another application that could greatly benefit from 5G. For now, driverless cars are self-contained, but in the future there are plans for them to communicate with other cars and smart roads to improve traffic and safety. In order for cars to successfully communicate with one another and road sensors while driving, there need to be instant data exchanges with minimal latency. The 1 ms latency rate of 5G could be critical to data exchanges and safety in these driverless car scenarios.
Unlike 4G networks, 5G will allow the use of small, inexpensive, low-power devices. This will open up options for IoT devices by allowing many more devices and entire cities to connect to the Internet. The low latency and high-powered speeds of 5G will also allow for phones to transform into virtual and augmented reality devices. The small cell design of the network will also help in-building coverage by allowing every home router to become a mini cell tower.
Before you start making plans to upgrade, take a deep breath, there aren’t any 5G devices on the market yet. And while your 4G devices won’t work on the 5G network, 4G LTE and Wi-Fi aren’t going away; they will be key factors in the 5G strategy and will actually perform better with the advances that will come with 5G. Wireless carriers are starting to work on the technology and there will be some pre-5G debuts taking place in 2017, but these won’t have all of the capabilities of a true 5G network. Plans for 5G are all still in the development process and the network is estimated to roll-out between 2018 and 2020. No matter when it officially comes to market, 5G will certainly be an exciting new frontier for wireless communication.