To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

Custom Cable Assemblies - One Size Does Not Fit All

cable assembly

Custom cable assemblies are something to consider. Have you ever worked on a new product design or network installation where an off-the-shelf product would not fit the bill? Did you find frustration as opposed to a readily available solution? Well, you’re not alone! Many of our customers come to us daily with custom cable requests to help them get their jobs done and to meet their customers’ critical deadlines.

As a manufacturer of cable assemblies, we make it a point to offer just about every type of cable assembly off the shelf. We stock cables with LSZH, Plenum, UV and Oil resistant jackets and more! We offer shielded and unshielded versions of cables, as well as IP67/68 rated assemblies for harsh environments. But even with our wide breadth of off-the-shelf cables we still manufacture a multitude of custom cable assemblies for our customers. Many times, the cable is being used by an OEM in a new product design where specific lengths and connector combinations are required.

So, whether you need an off-the-shelf cable, or a custom assembly never seen before, or coaxial cable tools, L-com has got you covered. Our ISO 9001:2015 manufacturing facilities in the US and China are ready to produce your custom cable built to your specs. We can build molded or assembled cables and offer a full suite of environmental and mechanical testing capabilities such as our Fluke toner test kits.  

For those of you who would prefer to make your own custom cable right now for fiber optic, coaxial or Ethernet applications, check out our easy-to-use online custom cable configurator. If you're still wondering what is coaxial cable then visit our blog post explaining this.

Or if you need a custom cable assembly with various coax connector types that our online configurator cannot provide call us at 1-800-341-5266 or e-mail us at sales@L-com.com for a custom product quote.

Resources

Search Entries