To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

Futureproofing with Cat6a Cable Assemblies

Cat6a Cable

There is no telling what technological breakthroughs await us in the future. But one thing no one wants, is to have to re-cable an entire network because the existing cabling can’t meet the speed and bandwidth needed to support future technology. Re-cabling consumes time, money and a lot of resources. So what is one to do to future-proof their cabling? For many, Cat6a is the answer.
 
Cat6a cables are high-tech cables with advanced performance standards for twisted pair cable systems that offer features surpassing other category cables. They offer more power, faster speeds, tighter twists, further distances, better shielding, and greater assurance that they’ll be able to keep up with today’s technology and future advancements. Cat6a cable assemblies are able to support upcoming advances in technologies such as Power over Ethernet (PoE), bandwidth-intensive applications and data transfers up to 10 Gbps. With 23-gauge twisted pair, they can transmit those 10 Gbps speeds over distances of up to 100m. Cat6a cables also feature shielding to control interference and crosstalk, which improves performance and increases operational bandwidth. While the extra shielding might add bulk to the cabling, the benefits of Cat6a far outweigh the increased costs that go along with a heavier cable.
 
In addition to PoE, there is a long list of technology coming to market that will continue to increase the need for speed and power. For example, next generation Wave 2 Wi-Fi devices will require 4 Gbps speeds in the near future. Enterprise businesses upgrading to this technology will be able to count on Cat6a to provide the speeds needed. HDBaseT is another emerging technology that would require Cat6a capabilities to transmit full, high-definition video, audio and data files over 100 meters. Plus, Cat6a cables can manage the data load needed to support IP convergence, which is beneficial to enterprise networking applications.
 
Overall, Cat6a might cost a bit more than Cat5e or Cat6 but investing in Cat6a now and its ability to keep up with the changing demands of new technology will save money in the long run. Check out our extensive selection of Cat6a cable assemblies.

Resources

Search Entries