To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

Blog posts tagged with 'ix-connector'

Benefits of the IX Industrial Ethernet Connector
The use of Ethernet cabling is only accelerating in industrial applications. A common occurrence with such applications is the need for a high number of parallel Ethernet connections in a small footprint, or just the ability to have more compact devices with Ethernet ports. The current standard Ethernet connector, the RJ-45 has been around for some time and is ubiquitous with Ethernet. However, this connector is considerably bulkier than is necessary and often suffers from retention issues without additional locking features.... Read more